Hi,
I made a board with the device of SN65HVD3083E and evaluated it.
However, due to the influence of noise on the signal line, I am considering adding the following contents to the circuit.
· Pull up A signal to 5 V with 10kΩ
· Pulldown B signal to GND with 10kΩ
· Pull up Z signal to 5 V with 10kΩ
· Pull down Y signal to GND with 10kΩ
* 5V is the VCC voltage.
I would like to ask about this content.
(1) Can the above contents reduce noise on the signal line?
(2) Does the above contents affect the device fail-safe function?
Best Regards,