Part Number: ISO5452
Hello guys,
One of our customer is evaluating ISO5452DW on their own board for their next products. They want to know the answers of the following questions. Could you please give me your answers?
1. What is the minimum pulse width of H level signal and L level signal at IN+/IN-? Is it 40ns?
2. If the minimum pulse width of H level and L level is 40ns, what is the output pulse width of OUTH/OUTL when H level or L level input signal with pulse width less than 40ns is input to IN+/IN-? Are OUTH and OUTL level not changed? the previous level is kept? Also is there any problem or malfunction when such short pulse signal is input?
3. When the customer uses ISO5452, do they need to filter the short pulse input signal less than 40ns?
Your answers would be appreciated.
Best regards,
Kazuya Nakai.