Part Number: DP83867IR
Hi Expert,
DP83867 offers both Strap & MDIO configuration for clock skew.
1. Register 0x0032 BIT0 and BIT1 determine whether clock skew enabled. The default value is "0", which means that clock is aligned with data. As a result, whether strap setup for RGMII_Clock_Skew is still available?
2. If both strap clock skew and MDIO clock skew are set to different value. e.g. Strap clock skew is 2ns with RX/TX[2:0] = 000; MDIO clock skew is 3ns with 0x0086 = 1011 for both transmit & receive clock skew. Which one will take effect, strap clock skew or MDIO clock skew?
Thanks.
Zhou