This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65986EVM: FTDI Connection

Part Number: TPS65986EVM
Other Parts Discussed in Thread: TPS65982, TPS65981, TPS65981EVM

Hi USB Team,

One of my customers is evaluating the TPS65986EVM ad having trouble connecting it to the Host Interface Tool via a FTDI FT232H dev board. No connection via either USB EP or FTDI to the Tool

What we have tried so far:

- Removed pre-installed FTDI drivers and installed the ones that come with the Host Interface Tool installation file (multiple times).

- Installed the Applications Customization Tool with included FTDI driver, no success.

- Followed instructions in the following E2E post (link) without any success. 

Questions:

-Does the TPS65982 driver that comes with the Host Interface Tool is the same as the TPS65986? Is the driver the same for the TPS6598 family?

- Any steps we may have missed? Suggestions moving forward?

EDIT:

-Customer is using Win10.