Part Number: TPS65982
Other Parts Discussed in Thread: , TPS65981EVM, TPS65981
Hello,
For a project with USB type C in alternate mode, I bought a TPS65982-EVM. For flashing a new firmware on the board, I tried to connect a ftdi-based adapter to the board over SPI and I²C.
All the user guides don't explain which FTDI chip is possible to communicate with the TPS65982 over the Application and Host Interface Tool. So I bought the module UMFT4222EV, that is possible to communicate with SPI or I²C devices over USB. I don't want to buy the expensive Aardvark I2C/SPI Host adapter with the same functionalities.
By connecting the FTDI module with the TPS65982-EVM and installing the correct FTDI driver, I still cannot communicate or flash the board. In the Application Tool I got this error message:
Exception Encountered during I2C Address Sweep:No FTDI I2C channels (I2C_GetNumChannels) detected, exiting....
<type 'exceptions.Exception'>
Traceback (most recent call last):
File "acConfigurationGui.py", line 2093, in sweep_handler
File "hw_interface.pyc", line 166, in hw_open
Exception
Is the FTDI module able to communicate over the TI Tools? If not, can you give me a list of possible modules?
Best Regards,
Jan Just