Part Number: TUSB546-DCI
Other Parts Discussed in Thread: HD3SS460, TPS65981
Dear Experts,
I have a Design with TUSB546_DCI and TPS65981. I would like to configure the EEPROM Content. I used the File for TPS65981 and HD3SS460 without success.
My ambition is a DFP, I configured the Power Rule (5V/3A) and the GPIO Pins (GPIO0: CTL1 / GPIO3: CTL0 / GPIO15: Flip). I made an export and flashed the EEPROM.
Now the USB Port works fine, the DP Port doesn't work. I measured these 3 GPIO pins and they are as follows:
CTL1 always High as soon as somthing is plugged. The flip pin is always low. CTL0 is low until a display port connector is plugged.
Nevertheless the flip logic seems to work, because it doesn't matter in which way I connect the USB Device.
My conclusion is, that the EEPROM Content is incorrect. Can you help?
Thanks in advance,
Bianca