We are using the TPD6F002 EMI filter extensively in our design. The datasheet shows a ground pad in the center of the device which we've included in our library component as pin 13 which is tied to ground. There are also two smaller pads on either end of the device. Should these pads be labeled as pin 14 and 15 and also tied to ground? They are not currently on our symbol so the pads are floating.