Looking at the datasheet for the TUSB2046B it states "Fully Compliant With the USB Specification as a Full-Speed Hub: TID #30220231". Does this mean it is USB 2.0 compliant?
The reference schematic uses SN75240 (USB port transient suppressors) that have in the datasheet "Note that the input capacitance of the device makes it unsuitable for high-speed USB 2.0 applications". Since the TUSB2540 is a full speed device, using the SN75240 in the design, is it USB 2.0 compliant??
-Tom-