Part Number: DP83867CS
Other Parts Discussed in Thread: DP83TC811S-Q1,
Hi Geet,
Thank you for the information about writing register 0x01D5 to reverse the SGMII polarity.
I was just testing it. I found that it didn't work until I issued a PCS reset by writing a 0x8000 to address 0x1000.
Can you please clarify some things about the DP83867 & its datasheet?
Did I do the right thing in asserting PCS_RESET to enable the SGMII polarity reversal? If I should follow a specific initialization sequence to properly invert the SGMII polarity, then please specify it.
When I set the inversion bits, I wrote a 0x3 to register 0x01d5 rather than setting each bit separately. Is this OK?
Page 42 of the March 2017 datasheet states MMD3 register is at 0x1000. Table 103 on page 91 states the register is at 0x0000, which doesn't make sense to me unless it's at a different MMD device address (other than 0x1f). Is this register aliased, or is the address in table 103 a typo?
Table 103 refers to both MMD3 and MMD7. The datasheet doesn't go into detail on these MMDs / registers. Can I find further information on MMD3 & MMD7 elsewhere?
Thank you again for your help.
Bob