Dear,
I am doing a Ethernet Compliance test on Fast Link Pulse (FLP) after we get issue with negotiations with some switched.
When the Ethernet compliance is done on DP83848K with LOAD1, LOAD2 and 50ohms only as specified in Ethernet all is good, but, when the Twisted Pair Model (TPM) is added before the load as specified in Ethernet standard for the compliance test, the FLP drops too much and the test fail.
What could be the root cause of such issue?
What parameter could helps to "boot" FLP pulse level and edges?
Sébastien