Other Parts Discussed in Thread: TMS320F28069, TCA9800, TCA9406
Hi,
I'm attempting to use ISO1540 for I2C isolation with a TMS320F28069.
I'm sending side 1 to the micro controller but it is having trouble communicating because of the 800mV logic low.
If I send a signal with a 500mV logic low (with another device), the communication goes thru and micro is able to transmit properly.
What can I do to improve the low logic on side 1 of the ISO1540 ?
A level shifter will only change the VDD level but not the ground level right ?
thank you