Part Number: TPS65987D
Hi TI,
we are using TPS65987D in our design. Please find attached block diagram. Our design takes power supply from two ways i) from USB type C adapter and ii) from battery.
We are using 'SWITCHING LOGIC' (MOSFET) to operate our system from outside supply (from USB type C) when it is present otherwise from battery voltage. For that voltage at point A must be greater than what is at B (which is 9V fixed from booster output).When this condition is fulfilled then A to C path is ON otherwise B to C will be ON.
In the datasheet of TPS65987D, section 9.2.1. "Under normal conditions, all high power PD contracts should start at 5 V and then transition to a higher voltage." is written. So,for my case Voltage at point A will be less than 9 V.
i)How it will scale up to a higher voltage? ii) Is this Voltage scale up dependent on system load? iii) Is there any way so that output of TPS65987D will be 12V after plugging in the supply from USB connector.
Thanks for reading.