Part Number: TPS65981
Other Parts Discussed in Thread: TPS65988, TPS65982
Hello TI Team,
we are using two TPS65981 PD controller in one device. One TPS65981 is a power sink, the other one is powered by the sink controller and acting as a power source. Buspowerz at the sink device is pulled-down by a resister to enable PP_EXT as input power path to power the entire system. Buspowerz at the source device is pulled-up by a resister to LDO_3V3 for disabling power from VBUS. That works! The normal operating voltage is set to 20V via PP_EXT only. I have two questions:
1. During first negotiation the sink controller provides 5V via PP_EXT to the entire system until the 20V contract is established. That will cause an over-current because of the quite high inrush current caused by some DCDC converters used. Is there any possibility to switch the external FET (PP_EXT) only when the 20V contract is established?
2. Both TPS65981 do have dedicated SPI flash memory. Is there a way to use the same flash image and just switch the configuration type (sink or source, etc) by a TPS65981 GPIO?
Thanks and Regards
Mario