This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953-Q1: filter parameter for high current POC appication

Part Number: DS90UB953-Q1

Hi, Team,

My customer need high current POC solution for CCD sensor solution. The power of the POC is 12V and >500mA. Do you have the design guideline for the filter parameter? Do we have the reference design for such application? Thanks!

  • Not, it is not recommended to have >500mA current through PoC. you can refer to www.ti.com/fpd-link on PoC theory train, with the current increase, the dynamic noise in the PoC is increased as well which would impact the link reliability as well. Also, the camera module would become hot due to high power consumption. Ti recommends the ISP is put in the de-ser side for lower power in the camera side.


    regards,
    Steven