Part Number: SN65HVD32
Other Parts Discussed in Thread: SN65HVD35,
Hi support team,
Our customer is considering RS-485 communication with switching full - duplex or half - duplex.
Therefore I am studying whether full-duplex RS-485 transceiver can be used as half-duplex transceiver.
I understand that the tranceiver with enable control of the driver and receiver such as SN65HVD35 is required.
But a port for enable control can't be prepared .
So I want to try to use the transceiver which is without enable control such as SN65HVD32 to the half duplex transceiver.
Because I think there is a possibility that the driver output may conflict, I am considering the following circuit diagram.
The resisters "Ri" are inserted to driver output of SN65HVD32.
Is there a possibility that this circuit can be used as a half duplex transceiver?
Also, please teach me if it has any precautions on use.
Sincerely,
M. Tachibana