Part Number: SN65DP141
Other Parts Discussed in Thread: HD3SS214
Hello.
I'm testing a prototype motherboard I designed with the SN65DP141 redriver fitted, which then drives into a DisplayPort switch. I can see what looks like valid DP signals at the input side of the redriver device, but all the outputs are static at +3.3V (device is powered from a +3.3V supply). I had neglected to fit AC coupling capacitors at the inputs and outputs, perhaps erroneously, on the basis that the device was fitted on the same board as the DP source, unlike the reference design which is for a stand-alone type of adapter. Should I have fitted these caps, particularly on the input side? Could their omission cause the outputs to be static at +3.3V, as if the device were in some sort of disabled state, or maybe without what it recognised as valid DisplayPort inputs? I have checked that the input to the PWD# pin is +3.3V.
Also, I've modified one of the prototype boards I have by removing the redriver device and linking the input pads to the output pads. With this modification the DisplayPort output (via the DP switch) works, suggesting that the DP source is ok.
I look forward to any replies. Thanks.