This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH1981: Output Terminal Current

Part Number: LMH1981

Hi, Team,

What is the maximum current value that can flow out from the output terminal?

If 1 KΩ terminating resistor is added to the HSOUT output of the pin, current of 3.3 mA (when VCC = 3.3 V) flows, is there no problem?
The maximum current value of the output pin was not found in the electrical characteristics table in the data sheet.

Best Regards,
Satoshi Yone