Part Number: TPS65982
I have the TPS65982 'Display Port Config (0x51)' register set to 'DP Port Capability' to 'UFP_D and DFP_D capable Device'.
The 'Enable Display Port SID' and 'Enable Display Port Mode' are set, as are 'C' and 'D' modes for the UFPD receptacle assignment.
When I connect my board to a Huawei phone it won't go into DisplayPort mode, even though the Display port status says it is all ok.
I have to change the Port Capability to 'DP UFP_D only' to get it to work.
WHY?? Other display port sources have no problem with this, such as PCs I connect to. It seems like if I negotiate that my board is an UF device, then the DF device should pick the correct display port mode and turn on.
Is the Huawei phone misbehaving?