This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB212: HS Signal quality fail - Eye shows rise time issue.

Part Number: TUSB212


Hi,

I am using TUSB212 for my HUB board and facing eye diagram failure.

My USB2.0 path has 2 muxes and one board to board connector.

Also attached Eye diagram for your reference.

Re-driver settings:

AC boost settings is maximum ( AC boost level = 3 -Did not mount any resistor on EQ)

DC boost settings is low ( Mid boost - 44K resistor on DC boost/ENS_HS pin)

Questions:

1)  I want to slightly increase AC boost  from AC boost level 3 ? if so Please share me the resistor value .

2)  what will happen if 10K is applied on EQ pin ? will rise time improve further ?

3)  What will be maximum  value of resistance that we can apply on EQ  pin for maximum EQ level for this IC Not  meant for level3 ?

4)  Why electrical characteristics table shows 6K resistor as minimum for AC boost level 3 and telling DNI on table for the same reason?

Regards

Regards

P.Vetrivel