This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HD3SS3220: For USB3.0 to type-C , I used in Camera , USB hub to Type-c ,Which mode should be set ? DFP?DRP? , For Power ,as PD ,5V is OK , is there needed power switch ? any advice?

Part Number: HD3SS3220


1/  I want use the HD3SS3220  as converter  the  USB3.0 to Type-c,  if the  HD3SS3220 could ok ?

2//for the Type-c POWER ,i need as PD ,5V is OK ,  if there need a power switch ? any device advice ? 

3//For  the HD3SS3220 , i used at camera ,Usb3.0 hub to type-c ,Which mode should be set ? DFP?DRP?UFP?  

4//if there any advice for USB3.0 to TYPE-C reference design ?