Part Number: TUSB2036
Hello,
I'm wondering the same thing as a previous post. In some TI examples, a 1.5k resistor is connected directly between DP0 and DP0PUR while others use an external NPN with the base connected the 5V from USB. When would you use on config over the other?
In my case, I have an embedded solution that has three USB devices on a single board, so I am using the TUSB2036 to provide one up-stream facing connector for the three devices. The TUSB2036 and USB devices have a 3.3V supply on the board and do not rely on the input USB 5V. It is also likely that the board will not always have the USB connection present, but I want it to enumerate when the USB is connected.
Can you please provide recommendations on the DP0PUR connections as well as RESETn? I'm planning on connecting the 15k + 1uF RC with the on-board 3.3V.
Thanks