Part Number: IO-EXPANDER-EVM
Other Parts Discussed in Thread: TCA6424A, , TCA9535, TCA9555, TMS320F28377S
I am beginning development on an application for the IO Expander TCA 9555 which controls various status LEDs and relays. To begin the initial development for our prototype, I have ordered the IO-EXPANDER-EVM which offers support for TCA 9555. According to the user's guide, the module comes populated with the TCA6424A and TCA9535.
I assume I will need to remove the TCA9535 and repopulate the board with TCA9555 for the application.
My question is:
1. Can I use this module as a standalone eval board for testing the I2C communication to TCA9555 and the response on the output ports? Is it possible to communicate to the repopulated chip without programming the firmware onto the module?
2. I will be using the TMS320F28377S LaunchPadXL for developing the I2C library. In case the firmware needs to be programmed, can I use this launchpad to do it?