Other Parts Discussed in Thread: SN65HVD1476, THVD1452
I'd like to implement a full duplex RS-482 bus. I'm thinking about using THVD1552 for the master and SN65HVD1476 for all slaves. I cannot use SN65HVD1476 for the master because there's only 5V available for power supply and the boards with slave transceiver already include SN65HVD1476. Will this configuration work fine?
I have seen that I could use THVD1452 both both master and slaves. Because I have selected VSSOP package, THVD1452DGS are not yet available. So this is only a future solution.
Thanks for your help