Part Number: SN75LVCP600S
Hi Sir
Customer use platform is Intel Skylake H. We can’t connection device when we use u20,u22(SN75LVCP600S). If we remove u20,u22. Then we can connect device.
May you have some suggestion can advise us?
Bogey
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN75LVCP600S
Hi Sir
Customer use platform is Intel Skylake H. We can’t connection device when we use u20,u22(SN75LVCP600S). If we remove u20,u22. Then we can connect device.
May you have some suggestion can advise us?
Bogey
Hi Sir
U100 U51 U70 U61 on Mother Board site,
U21 U19 U22 U20 on SSD Board site.
Our verify condition as below:
Condition 1: MB with U100 U51 U70 U61 and SSD Board with U19 U21 U22 U20 Function is OK.
Condition 2: MB with U100 U51 U70 U61 and SSD Board remove re-driver, Function is OK.
Condition 3: MB without re-driver and SSD with U21 U19 U22 U20, Funciton is Fail.
Hi Robert,
Condition 4: If you remove all the redrivers does the system fail?
If yes, the redrivers on the MB are the most important for system operation.
Regards,
Lee
Hi Robert,
Thanks for the feedback on this condition. I would try to probe the waveforms at the SSD to see how Condition 4 waveforms compare with the previous Condition 2 waveforms. It is likely there is improved margin using the SN74LVCP600. Based on the idea that the system can work without a redriver under "typical" conditions, I think cascading the redrivers would not ever be needed. In many cases cascading can have unforseen impacts on signal quality and is not recommended for most systems.
Regards,
Lee