Part Number: DP83869HM
Hi Sir,.
1.how` the TD_A_P/N definition in Table.6 mirror port configuration, if it was designed to RJ45 "PLUG" side ?
2. how`s the MDIO maximum clock definition ? is it correct for measurement 6ms/bit ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83869HM
Hi Sir,.
1.how` the TD_A_P/N definition in Table.6 mirror port configuration, if it was designed to RJ45 "PLUG" side ?
2. how`s the MDIO maximum clock definition ? is it correct for measurement 6ms/bit ?
Hi Philip,
Mirror mode changes the polarity and reorders the port numbers as well.
| Pin # (48QFN) | Mirror Mode Disabled Pin Assignment | Mirror Mode Enabled Pin Assignment |
| 1 | TD_P_A (A+) | TD_M_D (D-) |
| 2 | TD_M_A (A-) | TD_P_D (D+) |
| 4 | TD_P_B (B+) | TD_M_C (C-) |
| 5 | TD_M_B (B-) | TD_P_C (C+) |
| 7 | TD_P_C (C+) | TD_M_B (B-) |
| 8 | TD_M_C (C-) | TD_P_B (B+) |
| 10 | TD_P_D (D+) | TD_M_A (A-) |
| 11 | TD_M_D (D-) | TD_P_A (A+) |
MDIO max frequency is 25MHz.
-Regards
Aniruddha