This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65983B: VConn Not Powering to 5V when using Active Cable

Part Number: TPS65983B

Hello,

I am using TPS65983 Thunderbolt Application Customization 4.10, which uses based image TPS65983A_fw4_0004_59_00.bin

I configured the firmware with only one Source PDO, and it is using External High Voltage Power Path (PP_HVE) for 5V/3Amp power delivery.
I know the external FETs are wired correctly because I can negotiate PD and consume 5V/3A from my device, but when I tried an Active cable. I noticed on the PD analyzer that VConn is not powering to 5V, and therefore the link fails.

Is there a step in the firmware configuration I am missing?

Thank you