Part Number: DS90LV027A
Hi,
We are facing some Voltage Level issue with LVDS. In our case we have to setup an LVDS communication with an FPGA EVK to our DUT. DUT LVDS line is 2.5V. The FPGA pins which is available in FMC connectors is at 1.2V level. So we need to set this 1.2V single ended IOs to LVDS differential lines that can be communicate to 2.5V LVDS. We are planning to use DS90LV027A as LVDS driver, and SN74AVCT774 as level shifter ( FPGA end to driver input level shifting). Is it OK to connect the differential LVDS out from DS90LV027A driver to 2.5V LVDS differential line? ( Supply voltage of DS90LV027A is 3.3V, so does it swing at 3.3V?) Attaching a document regarding this issue. Please help....