Part Number: DP83TC811S-Q1
Dear team,
My customer recently test the PHY device. When they do the BCI test, there is a fault. The injection current is 100mA. The test frequency range is 1MHz to 100MHz. The frequency increases from 1MHz, and when it is increased to between 25M-30M, the communication between two PHY device is interrupted. At this time the log shows PHY error. Could you please help solve the problem?
The test circumstance is as below,
Thanks & Best Regards,
Sherry