This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TUSB2046B: Support for Bill of material

Part Number: TUSB2046B

Tool/software: TI C/C++ Compiler

Hi TI,

Now we would like to design 4-port USB 2.0 type A Hub.

We rely on your reference design with TUSB2046B.

However i can't seek Bill of material. I would like to have the part number of components in schamatic.

Please support me.

Thank8360.2046-PlainSelfPower.pdf

  • Hello Dinh Quang Thao,

    The TUSB2046B reference schematic is an older one from the 1990s and we do not have a BOM available.  It is likely even if we could find the original BOM, it would not longer be useful.  Do you have questions about specific components?

    Also, please be aware that the TUSB2046B is a USB 2.0 Full Speed Hub and does not support High Speed (480 Mbps) operation.

    Regards,

    JMMN