Hi Sir,
If SN65DSI86 clock source from DACP/N, then we need REFCLK pin mustbe tied pull-down to GND and 0x0A Bit0=1.
Do we still need to make other settings?
Hugo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hugo
Please refer to Table 1 of the DSI86 datasheet.
Please also note when using the REFCLK as the clock source, any DSI Clock frequency is supported, but if the clock source was instead the DSI A clock, then the required DSI Clock frequency would need to change to a frequency supported by the DSI86. When operating in this mode, any one of the following DSI A clock frequencies can be used: 384 MHz, 416 MHz, 460.8 MHz, 468 MHz, or 486 MHz.
Thanks
David