This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB941AS-Q1: column display is abnormal

Part Number: DS90UB941AS-Q1

Dear team,

SOC connected to 941 with dual DSI, deserial string is 948, 1920*720*60. the image is as below picture, looks like the lack of 1/2 column (there is a gap between the column and column, it seems that there is a missing column).

The customer setting 0x4F = 0x4C(Dual DSI, 4 lanes). PCLK=51MHz, DSI frequency is 165MHz.

When they read register, they found that there are two registers which are abnormal. Read 941 0x0C = 0x67, 0x5A = C9. And 0x5D=0x06.

Could you please help analyze this problem?

Thanks & Best Regards,

Sherry