Other Parts Discussed in Thread: SN65HVD72, THVD1410
Hi,
I have a question about the stub length of SN65HVD75. In an application I will connect 8 devices through RS485 bus,and using SN65HVD75 transceiver. Baud rate is 115200bps in the application. The stub length is 0.4m. I saw the requirment of the SN65HVD75 in datasheet is 0.05m, so I want to know the maximum stub length 0.05m if is the essential condition when transceiver runs on 20Mbps or any slower baud rate?