Part Number: TRS3232E-Q1
Hi TI-team
My customer wants to use TRS3232E-Q1 in half duplex.
Can it be used with a half-duplex line ?
Please answer the following questions when available.
1.What should the peripheral circuit be ?
2.Is Pull Up/Down necessary to fix the input side ?
3.I think it is necessary to connect the input and output with resistors.
How much protective element is required in the vicinity to protect the absolute maximum ratings In ± 25V and Out ± 13.2V ?
Best Regards,
Koji Hayashi