Other Parts Discussed in Thread: TUSB4020BI, TUSB217
Hi team
Can you recommend devices to improve the quality of USB 2.0 communication at a distance of 4.5 meters?
My customer met a problem that is when using a 4- or 4.5-meter USB shielded cable between two devices, only a few boards can correctly identify the device.
If changed 4- or 4.5-meter USB shielded cable to 2-meter USB shielded cable, all boards can successfully identify the device.
In order to achieve a communication distance of 4.5 meters, maybe a USB Hub or USB signal conditioner is a good choice.
My question is
- Can a USB signal conditioner (like TUSB213) address this issue?
- If the answer to question 1 is YES, how to understand the description in datasheet "supports up to 5m pre-channel or 2m post-channel Cable Length"? Does it mean that if place the signal conditioner (labeled as C in the following figure) near the B board (the distance is less than 2 meters), the distance from A board to signal conditioner can support up to 5 meters? If so, it seems that TUSB213 can meet the distance requirement.
- The USB hub can definitely solve this problem, right? Is TUSB4020BI a good choice?
Maybe I am asking some silly questions because I am not familiar with USB devices. Thanks for your patience.
Shawn Wang
shawn-wang@ti.com