Part Number: TPS65987D
Hello everyone,
my customer stated the following questions:
-----------------
I used the following GPIO event to communicate an overcurrent event via GPIO to the periphery:
GPIO5: "Port 0 Source Sink Event"
I notice the following behavior on this GPIO:
- when an overcurrent event (load resistance inserted) occurs, the GPIO is pulsed (see appendix)
- when the load resistor is removed, the GPIO remains set (high level)> is this behavior normal?
- When I unplug (not when plugging) various USB-C adapters, the GPIO is also set and remains set > is this behavior normal?
Can the GPIO (the corresponding bit) be reset via GPIO or via SW?
So far, I could only do this using the HRESET pin of the device.