Part Number: TUSB9261DEMO
Team,
on the schematic of TUSB9261DEMO, page 19, there is FB4 filter, C54, C64 and resulting voltage USB2_1P1V; then also filter FB5, C62, C58, C59, C61 and voltage VDDA_1P8V.
What are these two voltages meant for?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB9261DEMO
Team,
on the schematic of TUSB9261DEMO, page 19, there is FB4 filter, C54, C64 and resulting voltage USB2_1P1V; then also filter FB5, C62, C58, C59, C61 and voltage VDDA_1P8V.
What are these two voltages meant for?
Thanks!
1P1V means 1.1v and 1P8V means 1.8v.
Hi Brian,
thanks. I clicked that it resolved the issue, but in fact would need more explanation - from the VDD_1P1V (1.1v) that is used for 9261 supply, the USB2_1P1V is derived (after filter) - what for?
Secondly, from the crystal supply (BOARD_1P8V) from U4, the VDDA_1P8V is derived (after filter) - what for?
Hi Brian,
this is not what I was asking about. I was asking why do we create USB2_1P1V and VDDA_1P8V voltage rails in this schematic, as they do not seem to have any further connections on the schematic.
Can you please check and advise on that?
Thanks.