Our test structure would be as follows:
1. camera
2. Ser EVM (953A)
3. DeSer EVM (954)
4. Nvidia Jetson TX2
We know that the camera and the embedded board work together. (CSI-2, I²C and power coming in on the patch cord)
Does the 953/954 still have to be configured or do we only need to set the jumpers correctly to pass the video data through?
If configuration is necessary, are there standard configurations available?
We are interested in estimating the effort of programming.