Part Number: TCA9617A
Other Parts Discussed in Thread: TCA9517A, TCA9617B
Hi Sir,
Below is the schematic of TCA9617A which using to replace competitor PCA9617.
We found TCA9617 will pull low port A to 1V when DC off stage. (DC off stage means P3V3_STBY have power and P3V3 no power)
After DC on, we see port A pull to 3.3V, it is correct.
And then we DC off, we see port A keep at 3.3V.
We can’t read I2C address and it only occur at AC power on, TCA9617A will pull port A down to 1V.
Below is the waveform we captured.
Thanks