Hi,
The pattern checker consists of a 47-bit word counter and an 11-bit error counter. The pattern checker uses 32-
bit words. Hex 83 [2:0] and 84 [7:0]
Is there any way to increase # of error counter bits higher like 16 bits?
I see Hex 83 [7:3] bits are reserved.
I hope to be able to measure very high number of error count events like 1E-5, 1E-4, 1E-3.
Thanks,
Kilhun