This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953-Q1: Noise Reduction Methods

Part Number: DS90UB953-Q1


Dear Support member

The customer is to improve GPS receiver sensitivity on a system using DS90UB953.
A GPS module is implemented in the camera module.
The IMX390 (SONY image sensor) in the camera module is connected to the DS90UB953.

The GPS module has sufficient reception sensitivity.
When the IMX390 is operated, the C/NO value deteriorates by about 20 dBHz.

The IMX390 is set to Full HD (1080p) 20 Bit multi-exposure raw data at 30 FPS.
At this time, data rate is 371.25Mbps/lane × 4-lane.
This is the input to MIPI in DS90UB953.
When it is output from DOUT+ and DOUT- on the DS90UB953, it will be about 1485 Mbps (742 MHz) because it is added by 4-lane.

The frequency received by the GPS is 1575.42 MHz.
I assumed that the 2 times higher harmonic is close to the reception frequency of the GPS and is a noise factor.
Looking for the noise source with a loop antenna, we found that the noise level of the filter (PCMF3USB3S/CZ) where DOUT+ and DOUT- of the DS90UB953 are connected is high.
We tried to reduce the noise by adding a capacitor (22p) and beads (100 MHz, 120 Ω), but it was not an effective measure because it affected the FPD Link signal or was ineffective.

Q1.
If you have know-how on noise reduction (reference materials, etc.), please let me know.

Q2.
Please tell me if there are any noise reduction parts recommended for the FPD Link signal.

Best Regards,

  • Hi Mukku,

    The 953-954 pair actually runs at a fixed rate of 4Gbps (2GHz) regardless of the input bandwidth.

    I would suggest checking the power supplies and reference clock as well, since the FPD-Link rate is derived from the clock. In general, to reduce noise, you can consider adding EMC shield around the components, and make sure there's solid ground planes for the signal to return to, make sure the ground planes are stitched together. Adding decoupling caps to the power pins of the device can also reduce noise in the link.

    Best,

    Jiashow