Part Number: DS280MB810
Other Parts Discussed in Thread: DS280BR810
In the DS280MB810 datasheet (SNLS542, October 2016), the graphs on p. 13 in Section 6.7 show the gain transfer functions. The input differential peak-to-peak voltage is shown down to only about 250mVdpp, implying that the part may not properly handle input signals of smaller amplitude.
However, Tables 7, 8 and 9 on p.41-43, indicate 25.8Gbps input signalling being passed through input transmission lines having losses of 14dB and 22dB, which would result in input amplitudes far less than 250mVdpp.
How small an input signal will the device handle (ignoring such issues as squelch detect)? If less than 250mVdpp, why do the gain graphs not illustrate teh behavior for lower input amplitudes?