Part Number: TPS25750
(1) I would like a reference circuit diagram of TPS25750 with the following two conditions.
・ 5V / 3A (15W) Power Consumer (Sink)
・ 20V / 5A (100W) Power Consumer (Sink)
(2) I don't know the connection of the "PP5V" terminal.
・ 5V / 3A (15W) Power Consumer (Sink)
・ 20V / 5A (100W) Power Consumer (Sink)
Is it correct to disconnect the "PP5V" terminal when using the above two conditions?
(3) Does TPS25750 operate under the following two conditions without I2C control?
・ 5V / 3A (15W) Power Consumer (Sink)
・ 20V / 5A (100W) Power Consumer (Sink)
→ My hope is that the TPS25750 will work standalone.