Part Number: TCA9548A
Hello
I'm using TCA9548AMRGER 8 port USB HUB with following conditions
VCC = 3.3V, SDA and SCL are connected through pull-ups to the 3.3V.
The master selects only one of the channels at a time.
Can I connect different voltages to the pull-ups of the channels? For example: ch1 pull-ups to 1.8V, ch2 pull-ups to 2.5V, and ch3 pull-ups to 3.3V.
The recommended operation conditions (see datasheet on page 4) defines: high level input voltage as 0.7*VCC and low input voltage as 0.3 * VCC.
Does it mean that that the pull-up voltage shall be equal to VCC?
Regards