Part Number: DP83867IS
Hello,
I'd like to make sure I understand the magnetics requirements for the DP83867IS in order to implement a discrete solution that meets those requirements. The evalkits for this part seem to use HX5008NL for its discrete solution. This part's datasheet seems to indicate that its return loss is approximately -8dB at 100MHz, whereas your datasheet requirement seems to indicate that the test conditions for the part had a typical return loss of -10dB from 60MHz to 100MHz. Are the datasheet specifications really meant to be closer to guidelines?
I am thinking about using a part with similar specifications to HX5120NL. I believe this has the same return loss rating as HX5008NL, with worse crosstalk and CMRR performance that HX5008NL. The forum Q&A here https://e2e.ti.com/support/interface/f/138/t/504434 seems to indicate that this part is appropriate.
Overall, would I be able to use a part like HX5120NL? Should the datasheet requirements for the magnetics be adjusted or seen more as recommendations? I see the magnetics selection as something that's fairly dependent on the operating environment so I suspect a lot of it has to do with that, but having better guidelines for use with this specific set of magnetics would be good.
Thanks,
Matthew