Part Number: TPS65987D
Hi Team,
My customer considers using TPS65987D for his applicaton.
The application is like self-powered USB Type-C hub that has DC 24V input from AC adapter, and has upstream port USB Type-C connector.
If tablet PC is connected to the USB type-C connector, the expected behavior is the hub charges to the tablet PC with USB PD.
I believe the application is UFP(USB device) but wants to be source if AC adapter is connected.
To create new project by TPS6598x Configuration Tool, which port type should be selected for the application?
Best Regards,
Yaita