This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822I: Reducing Time from Cable Connect to Data Start

Part Number: DP83822I

I have a customer considering the DP83822 in a design.
They want to be able to reduce the time from a cable-connect event, to when data starts transmitting.

The below is a general understanding of how to do this:
- Disable Auto-MDIX; or Enable Fast-Auto-MDIX
- Disable Auto-Negotiation; or Enable Fast-Auto-Negotiation

From the DP83822 DS, it looks like both Fast-Auto-MDIX and Fast-Auto-Negotiation features are supported by the device.

Questions:

Could you give a general estimation of the expected reduction in time ("n" ms reduction, etc) for the following approaches?

1) Auto-MDIX and Auto-Negotiation are disabled
2) Fast Auto-MDIX is enabled; Auto-Negotiation is disabled (if enabling Fast Auto-MDIX, understanding is Auto-Negotiation needs to be disabled)
3) Auto-MDIX is enabled; Auto-Negotiation is disabled
4) Auto-MDIX is disabled; Fast-Auto-Negotiation is enabled
5) Auto-MDIX is enabled; Fast Auto-Negotiation is enabled

Or, if there is no time reduction due to the combinations listed above - what would be the expected reductions for changing the following parameters?

a) Auto-MDIX = disabled
b) Fast-Auto-MDIX is enabled
c) Auto-Negotiation is disabled
d) Fast-Auto-Negotiation is enabled

*For me, any help/advice on implementing such time-saving techniques, in addition to the above, would be much appreciated.*

Regards,
Darren

  • Hello Darren,

    The fast way to reduce the time from a cable connect to data transmittal would be disabling auto-MDIX and auto-negotiation, but without enabling the fast versions of them. 

    Sincerely,

    Gerome

  • Hi Gerome,

    Thanks for the feedback.

    Do you have any documentation that gives an example of a setup using the different configurations, and has some reference numbers on the reduction in link time and/or tradeoffs?

    Darren

  • Hello Darren,

    Linkup times will always be dependent on a myriad of variables within the system, such as cable quality, etc. What is the purpose of this inquiry? What is the use case?

    Sincerely,

    Gerome

  • Hi Gerome,

    I updated the use-case info in the "Notes" section - please see.

    Basically, the engineer wants to pick the best setup to achieve the fastest link time. 

    I understand that the time reduction is dependent on multiple system-level variables, and it is difficult to provide a time-reduction estimate.

    At the very least, could you rank the following setups in order of fastest-linkup to slowest-linkup?

    1) Auto-MDIX and Auto-Negotiation are disabled
    2) Fast Auto-MDIX is enabled; Auto-Negotiation is disabled (if enabling Fast Auto-MDIX, understanding is Auto-Negotiation needs to be disabled)
    3) Auto-MDIX is enabled; Auto-Negotiation is disabled
    4) Auto-MDIX is disabled; Fast-Auto-Negotiation is enabled
    5) Auto-MDIX is enabled; Fast Auto-Negotiation is enabled

    Thanks,

    Darren

  • Hi Darren,

    The order you have listed is the order from fastest to slowest, according to our estimates. Please keep in mind that with in option 2, robust and regular auto-mdix need to also be enabled. Option 3, robust auto-mdix also needs to be enabled. Please keep in mind that this is theoretical, and that these configurations have not been tested, so a bench validation would be needed on the customer side.

    Sincerely,

    Gerome