Other Parts Discussed in Thread: ASH, , TPS65988
Hi all,
I was wondering if it was possible to create a Bi-Directional combined Usb C sink / source device. Hopefully it would have just a single type c connector on one side and a dc connector on the other.
Ideally I would like it to be able to take a voltage eg: 12-20v in and be able to output 5v/9v/15v/20v on the USB C port as well as passing through power from a USB C source to a Dc output ie: select 5v/9v/15v/20v and have it output that to a Dc connector from a USB C power bank / wall adapter.
Is there a chip that can do this and auto negotiate or would it even be possible to use two USB C Pd controller's back to back?
Thanks all, and apologies for any errors or issues.