This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25750: VBUS input without CC1/CC2 connected

Part Number: TPS25750

Hi team,

Customer is using TPS25750, and due to their application requirement, they are checking with us to see if they could connect a 5V to VBUS_IN directly and left CC1/CC2 floating, and get 5V/3A power from PPHV. Could you help comment if this is a workable method?

Thanks and best regards,

Will