Part Number: DS90UB949-Q1
Hi team,
for UB949 REM_INTB and INTB, what's the difference between them? In the datasheet, only say the that Remote interrupt. Mirrors status of INTB_IN from the deserializer. Note: External pullup to 1.8 V required. Recommended pullup: 4.7 kΩ
for the INTB, also say it is remote interrupt. I know if use INTB, need read reg C7 to clear it, while use REM_INTB, it not need be clear. any others?
can I understand that INTB can be used as local and remote slave status, but the REM_INTB only for remote.?
if we use REM_INTB, can we left INT_B float, or need pull up to 1.8V. Can we connect the INTB and REM_INTB together?
thank you