Part Number: DS280DF810
Hello,
i'm trying to design an universal board.
Looking from the board's point of view there are three families of 25G 8-channel devices: BR, MB and DF.
These families differs only within the following pins: D4, D12, E2, E4, E14, F4.
In my case the MUXSEL pins on MB family are not needed since it will be controlled through I2C.
All other pins are GND and/or TEST pins.
Datasheet says that TEST pins should be tied to ground in normal (non-test) operation.
Can i connect all these pins directly to GND without pulldown resistors?
Thank you.